(!)NOTE : Windows 7 users won’t be able to use some latest features of eCatalog/WOS since Microsoft is ending support for Windows 7 on 14 Jan, 2020. Please upgrade your system for uninterrupted services.

Understanding Plated Bolts: How Different Coatings Affect Performance and Applications

Categories:

Fasteners

Publish Date: 13 Mar 2026

If you look closely at fasteners used in machinery, construction, or equipment assembly, you’ll notice that bolts often appear in different colors—matte silver, shiny silver, black, yellow, or even rainbow-like finishes. These colors are not just for appearance; they indicate the type of surface plating applied to the bolt.

Surface plating plays an important role in determining how a bolt performs in different environments. From rust prevention and corrosion resistance to durability and visual finish, the coating on a bolt can significantly influence where and how it should be used.

Understanding the different types of plated bolts helps engineers, maintenance teams, and procurement specialists choose the most suitable fasteners for their applications.

Understanding Plated Bolts: How Different Coatings Affect Performance and Applications

Why Is Bolt Surface Plating Necessary?

Surface plating or coating is used to enhance the performance and durability of fasteners. Since bolts are often exposed to environmental conditions such as moisture, chemicals, heat, and friction, coatings provide an extra protective layer.

Depending on the coating type, plated bolts can offer benefits such as:

  • Improved corrosion resistance
  • Protection against rust and oxidation
  • Increased abrasion and wear resistance
  • Better heat tolerance
  • Enhanced surface hardness
  • Improved visual appearance

Choosing the right plating ensures that the bolt performs reliably in its intended environment while maintaining structural integrity.

6 Popular Bolt Coatings Used in Industry

Many plating options are available in the market today, each designed for specific working conditions. Below are six commonly used bolt coatings and their typical applications.

1. Zinc-Plated Bolts

Zinc plating is one of the most widely used coatings for bolts and nuts. The process uses electrical current to deposit a thin zinc layer onto the fastener surface. This layer acts as a protective barrier that slows rust formation.

Zinc plating is available in several finishes:

Zinc-Plated Bolts
  • White zinc
  • Yellow zinc (rainbow zinc)
  • Black zinc

Precautions

Zinc-plated bolts are not ideal for outdoor or highly humid environments, as the thin coating can corrode over time.

Common Applications

  • Vehicle components
  • Indoor structural assemblies
  • General machinery fastening

Because of its affordability and versatility, zinc plating is commonly used for general industrial applications.

2. Hot-Dip Galvanized Bolts

Hot-dip galvanizing (HDG) involves immersing bolts and nuts in molten zinc, creating a thick protective coating typically 40–65 microns thick—much thicker than electroplated zinc.

This coating provides excellent resistance to corrosion, especially in harsh outdoor environments.

Hot-Dip Galvanized Bolts

Precautions

Due to the thick coating, hole tolerances must be considered when using these bolts. Additionally, they should not be used in plumbing systems due to possible zinc contamination.

Common Applications

  • Outdoor structures
  • Electrical poles
  • Structural installations
  • Chemical processing environments

HDG bolts are often chosen for projects where long-term corrosion protection is required.

3. Zinc Flake Coated Bolts

Zinc flake coating uses a zinc-aluminum compound applied to the bolt surface, resulting in a thin gray protective layer (approximately 8–12 microns thick).

Despite being thinner than HDG coatings, zinc flake coatings provide excellent corrosion resistance, heat resistance, and chemical stability.

Another advantage is that the process is environmentally friendly, as it avoids hazardous substances.

Zinc Flake Coated Bolts

Precautions

Similar to galvanized coatings, zinc flake coated bolts are not recommended for water supply or plumbing systems.

Common Applications

  • Automotive manufacturing
  • Shipbuilding
  • Structural applications requiring high durability

These coatings are commonly used when high corrosion resistance and environmental compliance are required.

4. Black Oxide (Blackened) Bolts

Black oxide coating is created through a chemical reaction with the steel surface, producing a thin black oxide layer. This coating offers mild corrosion resistance while maintaining the original dimensions of the bolt.

It is also a cost-effective finishing method and gives bolts a clean, professional appearance.

Black Oxide (Blackened) Bolts

Precautions

Blackened bolts should not be used in humid or outdoor environments, as they offer limited rust protection.

Common Applications

  • Tool assembly
  • Machinery components
  • Steel structural assemblies

They are often coated with oil or paint afterward to enhance corrosion resistance.

5. Chrome-Plated Bolts

Chrome plating involves coating bolts with chromium using electricity and heat, resulting in a bright and highly durable surface.

Benefits include:

  • Excellent scratch resistance
  • Improved corrosion protection
  • Attractive mirror-like finish

There are two main types:

  • Trivalent chromium (Cr3+)
  • Hexavalent chromium (Cr6+)

While Cr6+ offers a brighter finish and lower cost, it is toxic and requires strict environmental controls.

Chrome-Plated Bolts

Precautions

Chrome-plated bolts should not be used in environments with strong acids or alkalis.

Common Applications

  • Decorative automotive components
  • Furniture hardware
  • Machinery parts requiring aesthetic appeal

Chrome plating is often selected when appearance and durability are equally important.

6. Nickel-Plated Bolts

Nickel plating provides a durable protective layer that enhances corrosion resistance while improving electrical conductivity and surface hardness.

Nickel coatings are available in:

  • Electrolytic nickel plating
  • Electroless nickel plating (EN)

Electroless nickel plating is more expensive but offers uniform coating thickness and superior corrosion resistance.

Nickel-Plated Bolts

Precautions

Nickel-plated bolts should not be exposed to highly acidic or alkaline environments.

Common Applications

  • Electrical equipment connections
  • Battery terminals
  • Household appliances
  • Furniture and bathroom fixtures

Nickel plating is commonly used where electrical performance and corrosion protection are important.

Choosing the Right Plated Bolt for Your Application

As seen above, different bolt coatings provide different levels of corrosion resistance, durability, and performance. When selecting plated bolts, it is important to consider factors such as:

  • Environmental conditions
  • Exposure to moisture or chemicals
  • Mechanical load requirements
  • Cost considerations
  • Desired appearance

Selecting the right coating ensures that the fastener will perform reliably and maintain long service life.

Find Reliable Fasteners at MISUMI

Choosing the correct bolt coating is an important step in ensuring durable and reliable assemblies. Whether you need zinc-plated bolts for general machinery, galvanized fasteners for outdoor structures, or specialty plated bolts for demanding environments, selecting high-quality components is essential.

Explore MISUMI’s wide range of fasteners, including plated bolts, nuts, and precision fastening solutions designed for industrial applications. With MISUMI, you can find the right fasteners quickly and confidently for your engineering and manufacturing needs.

Published By

Rupali Sharma

Share on:

whatsapp-qr whatsapp-icon