(!)NOTE : Windows 7 users won’t be able to use some latest features of eCatalog/WOS since Microsoft is ending support for Windows 7 on 14 Jan, 2020. Please upgrade your system for uninterrupted services.

  • We are upgrading our website for a better purchasing experience. Stay tuned for more updates! Know more
  • IMPORTANT: Please remember your log-in details, as you need to re-log in post the website upgrade. Reset in case: Forgot log-in ID OR Forgot Password

Photomicrosensors Explained: Their Structure, Material Use, and Sensor Types

Categories:

Sensors

Publish Date: November 02, 2025

Introduction

Photomicrosensors are compact, highly reliable photoelectronic sensors specialized for precise object detection and positioning in various equipment and industrial applications. Known commonly as photointerrupters, these sensors detect objects using an optical beam, which can be interrupted or reflected, generating signals for automation and control systems. This article explains their structure, materials, uses, and sensor types, offering a comprehensive overview for engineering professionals and technical content creators.

Photomicrosensor Structure and Working Principle

A photomicrosensor typically consists of two main semiconductor components: an emitter (usually an infrared LED) and a photo detector (often a phototransistor or photodiode) paired with a built-in amplifier circuit. This integration makes them highly sensitive and compact devices suitable for embedding into equipment.

There are two primary structural types:

  • Transmissive (Slotted) Photomicrosensors:
    Features an emitter and detector placed opposite each other across a narrow slot or aperture. Object detection occurs when the object passes through the slot, physically interrupting the light beam. This interruption changes the amount of light reaching the detector, generating a switching signal. Ideal for detecting opaque objects and precise positioning because of stable and repeatable detection.
  • Reflective Photomicrosensors:
    Both emitter and detector face the same direction. Detection relies on the reflection of light off an object back to the detector. Suitable for sensing object presence, absence, or surface markings without needing the object to physically block a beam. Enables low-profile, flexible installation designs.

Photomicrosensors are mainly built using semiconductor materials such as gallium arsenide (GaAs) or gallium aluminum arsenide (GaAlAs) for the LED emitter and silicon-based phototransistors for detection. Protective housings are designed for dust resistance and to limit interference from ambient light, sometimes incorporating filters against visible light for stable operation.

Common Uses and Applications

Photomicrosensors are widely used in automation, electronics, and precision equipment. Their compact size and reliable detection capabilities make them indispensable in:

  • Object presence and absence detection in manufacturing lines.
  • Disk rotation counting and direction sensing in rotary encoders.
  • Positioning moving parts precisely in machinery and robotics.
  • Detecting open/closed states such as machine covers or doors.
  • Mark detection on printed circuit boards or paper sheets.
  • Consumer electronics applications like ATMs, printers, and smart meters.

Various application-specific configurations allow photomicrosensors to be embedded into constrained spaces where traditional photoelectric sensors would be too bulky.

Types of Photomicrosensors

Type Description Typical Use Cases
Transmissive (Slot) Opposed emitter and detector; detects beam interruption. Object counting, positioning, door/cover sensing.
Reflective Emitter and detector on the same side; detects reflected light. Presence detection, mark sensing, proximity sensing.
Retroreflective Detects light reflected back from a reflector on opposite side. Medium-range detection with fewer false signals.
Modulated Light Uses modulated infrared light to reduce ambient noise interference. High-precision sensing in noisy environments.

Conclusion

Photomicrosensors are essential components for precise, reliable object detection and positioning in modern automation and consumer equipment. Their compact structure, built-in amplifiers, and versatile sensing principles (transmissive and reflective) allow integration into tight spaces and diverse applications. Understanding their materials, structure, and types helps engineers select the right sensor to optimize performance in industrial and electronic systems.

This detailed overview provides a solid foundation for writing technical content or making informed product choices involving photomicrosensors in sophisticated automation environments.

Published By

Vishal Dhara

Share on:

whatsapp-qr whatsapp-icon