(!)NOTE : Windows 7 users won’t be able to use some latest features of eCatalog/WOS since Microsoft is ending support for Windows 7 on 14 Jan, 2020. Please upgrade your system for uninterrupted services.

How Safety Light Curtains Improve Safety in Press and Robot Systems

Categories:

Sensors

Publish Date: November 2, 2025

Safety light curtains significantly improve safety in press machines and robotic systems by providing a non-intrusive, flexible, and highly responsive protective barrier that helps prevent accidents and injuries in hazardous industrial environments.

Enhanced Worker Protection

Safety light curtains create an invisible sensing screen using multiple infrared light beams positioned around hazardous zones, such as presses or robot workcells. If any object, such as a hand or arm, breaks these beams, the light curtain immediately signals the machine to stop operation, preventing contact with moving parts, crush points, or pinch hazards. This rapid detection and shutdown avoid injuries and fatalities, offering superior protection compared to traditional physical guards and manual controls. For instance, in press operations involving heavy force, light curtains can prevent the press from cycling if a worker’s arm encroaches on the danger zone.

  • Immediate detection of human presence in danger zones
  • Prevents accidents by stopping machines instantly
  • More sensitive and reliable than physical barriers

Non-Intrusive and Flexible Safety Solution

Unlike hard guards or fences, light curtains do not obstruct the operator's view or movement, allowing better visibility and easier access for material handling, maintenance, or tool changes. This flexibility enhances productivity by speeding up workflow and minimizing downtime. Light curtains can be customized in size and beam resolution to suit different machine types and configurations, making them ideal for diverse industries like automotive manufacturing, packaging, CNC machining, and robotic cells.

Integration with Robotic Systems

In robot systems, safety light curtains act as an essential safeguard by defining a protective perimeter around robotic cells. When the curtain detects intrusion, it immediately halts robot operation, protecting workers from fast-moving robotic arms and automated handling. This safety device enables close collaboration between humans and robots without the physical restrictions of cages, facilitating safer and more efficient human-robot interaction in automated production lines.

Compliance and Cost Effectiveness

Safety light curtains assist manufacturers in meeting strict safety regulations and standards such as ISO 13849-1 and OSHA requirements. By reducing workplace injuries, machine downtime, and legal liabilities, these devices also deliver substantial cost savings over time. Their easy installation, robust design, and minimal maintenance further enhance their return on investment compared to mechanical guards.

Summary of Benefits in Press and Robot Systems

Benefit Description
Enhanced Safety Immediate machine stop when a light beam is interrupted, preventing operator injury
Non-Intrusive Allows clear visibility and easy access without physical obstructions
Flexibility Customizable size and beam settings for various applications
Improved Productivity Reduces downtime by enabling fast, safe operations and easy maintenance
Integration with Robots Safe human-robot collaboration by quickly stopping operation if safety zone is breached
Regulatory Compliance Helps meet safety standards and reduces legal exposure
Cost Efficiency Lowers injury-related costs, maintenance expenses, and installation complexity

Conclusion

In conclusion, safety light curtains are a critical safety technology for modern press machines and robotic systems. They provide a reliable, flexible, and efficient protective solution that safeguards operators, enhances operational efficiency, and ensures regulatory compliance in industrial environments.

Published By

Vishal Dhara

Share on:

whatsapp-qr whatsapp-icon