How Rotary Encoders Ensure Accurate Position and Speed Measurement
Publish Date: Sunday, November 02, 2025
Rotary encoders are essential components in many automation and control systems, used for precisely tracking the position and speed of rotating shafts. By converting mechanical rotation into electrical signals, rotary encoders enable machines to know their exact angular position and velocity, which is critical for precision control in robotics, manufacturing, and various motion systems.
What Is a Rotary Encoder?
A rotary encoder is a sensor that provides feedback on the angular position of a rotating shaft. It consists mainly of a coded disk attached to the shaft and one or more sensors that read the disk's pattern as it spins. This feedback can then be used to determine the shaft’s position and rotational speed.
Types of Rotary Encoders
- Incremental Encoders: These generate a series of pulses as the shaft rotates. Counting these pulses and determining their timing provides relative position and speed data. Incremental encoders do not provide absolute position immediately after system startup but track movement relative to a known point.
- Absolute Encoders: These assign a unique digital code to each shaft position, providing an absolute position value instantly upon power-up without needing to reference a zero point.
How Rotary Encoders Measure Position
- Optical Encoders: A disk with transparent and opaque segments rotates between an LED light source and photodetector. As the disk turns, the photodetector senses light interruptions, generating electrical pulses. These pulses correspond to specific shaft positions.
- Magnetic Encoders: A magnetized disk rotates near a sensor such as a Hall-effect device. Changes in the magnetic field as the disk rotates generate signals that represent the shaft’s position.
Signal Processing for Accuracy
Encoders create signals that are processed by motion controllers or digital readouts. Incremental encoders typically output two square wave pulses 90 degrees out of phase, known as quadrature signals. Analyzing these pulses allows the determination of both position and direction of rotation. Counting every rising and falling edge of these signals increases resolution.
Absolute encoders output a coded digital signal that directly corresponds to each discrete position angle, enabling precise position determination without cumulative counting errors.
Measuring Speed with Rotary Encoders
Speed measurement is achieved by counting pulses over a known time interval. The number of pulses corresponds to how far the shaft has turned, and the time interval gives the rotational speed. High pulse density (Pulses Per Revolution or PPR) encoders provide finer resolution and more accurate speed readings.
In real-time control systems, accurate speed measurements allow the control system to adjust motor performance dynamically, ensuring smooth and precise motion even under changing loads or conditions.
Ensuring Accuracy in Position and Speed Measurement
- High Resolution: Increasing the number of pulses per revolution improves the precision of position and speed measurements.
- Signal Quality: Use of shielded cables, differential signaling, and filtering reduces noise from electrical interference.
- Proper Calibration: Aligning the encoder with the shaft and routinely checking calibration maintain accuracy over time.
- Mechanical Quality: Well-manufactured scales or disks with precise markings reduce cyclic errors.
- Environmental Protection: Magnetic encoders perform well in dirty or harsh environments, while optical encoders require clean conditions.
Applications and Benefits
Rotary encoders play a key role in applications requiring precise position and speed control such as CNC machines, industrial robotics, automated assembly, and packaging systems. Their precise feedback helps achieve high-speed operation, repeatability, and process efficiency.
MISUMI India Product Example
One example of a high-quality rotary encoder available from MISUMI India is the MISUMI Incremental Rotary Encoder. This product offers precise position and speed measurement capabilities suitable for diverse industrial automation applications.