(!)NOTE : Windows 7 users won’t be able to use some latest features of eCatalog/WOS since Microsoft is ending support for Windows 7 on 14 Jan, 2020. Please upgrade your system for uninterrupted services.

How Stepping Motors Improve Positioning Accuracy in Automation Systems

Stepper motors improve positioning accuracy in automation systems through their inherent design that divides rotation into precise discrete steps, their ability to be finely controlled via pulse frequency and microstepping, and their strong holding torque that maintains position stability. These features enable stepper motors to deliver highly repeatable and exact movements without the need for complex feedback systems, making them ideal for applications requiring precise control of motion.

How Stepping Motors Achieve Positioning Accuracy

Stepper motors rotate in fixed angular increments called steps, typically 1.8 degrees per step, equating to 200 steps per revolution. This division of rotation into discrete steps allows for predictable positioning, as each pulse sent to the motor controller corresponds to a specific step movement. The direct correlation between input pulses and rotor position gives stepper motors their intrinsic accuracy in open-loop systems, eliminating the need for position sensors or feedback loops that complicate servo motor systems.

Microstepping for Enhanced Precision

To further refine positioning, microstepping divides each full step into many smaller microsteps, typically up to 256 microsteps per step, reducing the step angle to as low as 0.007 degrees. This technique not only increases the resolution of the motor's movement but also smooths operation, reducing mechanical vibrations and cogging at low speeds. Microstepping significantly enhances the accuracy and smoothness of positioning, enabling precise control in applications such as robotics, CNC machinery, and semiconductor equipment.

Strong Holding Torque and Stability

Stepper motors generate a strong holding torque when stationary, which helps maintain their position reliably against external forces. This magnetic holding force ensures the motor shaft remains precisely in place without oscillations or drift, a key advantage in automation systems requiring stable, repeatable positioning.

Advantages in Automation Systems

Open-Loop Control Simplicity: Stepper motors do not require position sensors or complex feedback systems, simplifying the automation system design and reducing costs.

Predictable and Repeatable Steps: Each pulse corresponds to a precise angular movement, enabling easy programming of exact positions.

Resistance to Position Jitter: Unlike some servo systems that can oscillate around set points, steppers hold positions firmly without dithering.

Good Low-Speed Torque: Maintaining torque even at low rotational speeds supports precise positioning without losing control.

Fault Tolerance in Stall Conditions: Stepper motors will stall without damage if overloaded, avoiding errors that might damage the system.

Practical Applications

Stepper motors are widely used in automation fields where precision positioning is critical without the cost or complexity of servo motors. Common use cases include 3D printers, CNC routers, robotic arms, packaging machinery, and semiconductor manufacturing, all benefiting from the stepper motor’s ability to deliver accurate, repeatable positioning.

Conclusion

In summary, the discrete step motion, microstepping capability, strong holding torque, and open-loop simplicity of stepping motors combine to improve positioning accuracy in automation systems. Their reliability and ease of integration make them a preferred choice in many precision motion control applications.

This comprehensive understanding is supported by detailed technical resources and industrial experts emphasizing the role of stepping motors in delivering precise and stable positioning in automation environments.​

Published By

Vishal Dhara

Share on:

whatsapp-qr whatsapp-icon