(!)NOTE : Windows 7 users won’t be able to use some latest features of eCatalog/WOS since Microsoft is ending support for Windows 7 on 14 Jan, 2020. Please upgrade your system for uninterrupted services.

Mitutoyo Surface Roughness Testers: What You Should Know Before Measuring Surface Finish

Categories:

Measuring Tools

Publish Date: 11 Mar 2026

In machining and manufacturing, surface finish directly affects part performance, friction, wear resistance, and sealing ability. Even when a component appears smooth, microscopic peaks and valleys may still exist.

To measure these variations accurately, manufacturers rely on Mitutoyo Surface Roughness Testers, widely used for quality inspection in machining, automotive, and electronics production. Available through MISUMI, these testers help engineers quickly verify whether a surface meets the required roughness specifications such as Ra or Rz.

How Mitutoyo Surface Roughness Testers Measure Surfaces

Mitutoyo surface roughness testers typically use a stylus tracing method.

A small stylus tip moves across the surface of the workpiece. As the stylus passes over peaks and valleys, the vertical motion is converted into electrical signals. The instrument processes this signal and generates a surface profile and roughness parameters.

Most portable testers such as the Mitutoyo Surftest series support:

  • Primary profile measurement
  • Roughness profile analysis
  • Waviness profile evaluation

These profiles allow engineers to distinguish between true surface roughness and larger surface deviations caused by machining conditions.

Surface roughness measurement process using a stylus probe and signal processing system.

Mitutoyo testers also comply with international standards including ISO, ANSI, and JIS, ensuring measurement results match global inspection requirements.

Surface Roughness Parameters Customers Commonly Check

While many roughness parameters exist, most manufacturing drawings specify only a few key ones.

Ra – Average Surface Roughness

Ra is the most commonly specified roughness parameter. It represents the average deviation of the surface profile from the mean line.

Typical uses:

  • General machining inspection
  • Turning and milling surface checks
  • Production quality verification

Rz – Maximum Height of Profile

Rz measures the difference between the highest peak and lowest valley within the evaluation length.

This parameter is often used for:

  • Functional surfaces
  • Wear-sensitive components
  • Sealing areas

Rq – Root Mean Square Roughness

Rq provides a statistical evaluation of the surface profile and is sometimes used when more sensitive surface analysis is required.

Mitutoyo surface roughness testers can calculate dozens of parameters including Ra, Rz, Rq, Rsk, and Rku, allowing the instrument to support different measurement standards and applications.

Why Sampling Length Matters in Surface Measurement

One factor customers often overlook is sampling length, which determines how much of the surface is analyzed during measurement.

If the sampling length is too small, the measurement may miss larger surface variations. If it is too large, waviness may influence the roughness value.

International standards recommend selecting sampling length based on expected roughness ranges. Common cutoff values include:

  • 0.08 mm
  • 0.25 mm
  • 0.8 mm
  • 2.5 mm

Using the correct sampling length ensures consistent and repeatable surface roughness measurements.

Key Features of Mitutoyo Surface Roughness Testers

Customers typically choose Mitutoyo testers for their accuracy, portability, and measurement flexibility.

Common features include:

  • High measurement resolution (up to 0.002 µm in some models)
  • Multiple roughness parameter calculations
  • Color LCD display for profile visualization
  • Built-in data storage and statistical analysis
  • USB or SPC output for data transfer
  • Portable operation for shop-floor inspection

These features allow the tester to be used both in production lines and in quality control laboratories.

Typical Applications

Mitutoyo surface roughness testers are widely used across industries for surface finish verification.

Common applications include:

  • Machined metal parts
  • Automotive components
  • Precision mechanical parts
  • Semiconductor equipment components
  • Medical device manufacturing

In many production environments, roughness testers are used alongside calipers, micrometers, and CMM inspection tools as part of a complete quality inspection process.

Surface Measurement Solutions Available Through MISUMI

Mitutoyo surface roughness testers provide reliable measurement of surface finish parameters required in modern manufacturing. By accurately measuring Ra, Rz, and other roughness parameters, these instruments help ensure components meet design specifications.

Through MISUMI, engineers can access Mitutoyo’s precision inspection equipment to support machining quality and production reliability.

Published By

Rupali Sharma

Share on:

whatsapp-qr whatsapp-icon