(!)NOTE : Windows 7 users won’t be able to use some latest features of eCatalog/WOS since Microsoft is ending support for Windows 7 on 14 Jan, 2020. Please upgrade your system for uninterrupted services.

A Complete Guide to Using Mitutoyo Dial Indicators

Categories:

Measuring Tools

Publish Date: 21 Jan 2026

You know that feeling when you are trying to figure out if a metal surface is perfectly flat or if a rotating shaft has the tiniest wobble, but your eyes just aren't sharp enough to see the difference? That is exactly why the dial indicator was invented. It takes those invisible physical deviations and turns them into a needle movement you can actually see and measure with incredible precision.

Whether you are checking for "run-out" on a lathe or aligning a machine, the mitutoyo dial gauge is the industry standard for getting the job done right.

Complete Guide to Using Mitutoyo Dial Indicators

What Is a Dial Gauge Indicator and Why It Is Used?

A dial gauge (dial indicator gauge) is a precision instrument used to measure small linear displacement relative to a reference surface. Unlike calipers or micrometers, a dial gauge does not measure absolute size—it measures variation.

A dial gauge Mitutoyo is commonly used for:

  • Checking runout and concentricity
  • Measuring flatness and parallelism
  • Aligning machine components
  • Monitoring deflection during load or motion

Because these measurements directly affect fit, function, and repeatability, dial indicators are widely used in quality control, machine setup, inspection, and maintenance.

Understanding the Parts of a Dial Gauge Mitutoyo

Before you start measuring, you need to know what you are looking at. A dial indicator mitutoyo consists of several precision-engineered parts that work together to translate linear movement into a circular reading.

  • The Dial Face: This is where you see the results. It includes the hand (pointer) and often a smaller revolution counter.
  • The Bezel and Bezel Clamp: The outer ring can be rotated to "zero" the gauge, and the clamp locks it in place.
  • Limit Markers: These small physical tabs can be set to show your acceptable tolerance range at a glance.
  • The Stem and Spindle: The stem is the mounting point, while the spindle (or plunger) is the part that actually moves up and down.
  • Contact Point: The very tip that touches your workpiece. These are often replaceable depending on the surface you are measuring.
Understanding the Parts of a Dial Gauge Mitutoyo

How to Read Dial Gauge Indicators Correctly

Not every dial gauge indicator reads the same way. Depending on your specific task, you might be using one of three common dial faces:

How to Read Dial Gauge Indicators Correctly
  • Continuous Dial: Used for direct reading. The numbers continue around the entire face.
  • Balanced Dial: Used for reading the difference from a reference surface. The “0” is at the top, and it shows plus or minus deviations.
  • Reverse Reading Dial: Typically used for depth or bore gauge measurements.

When performing a dial gauge reading, always look at the small revolution counter first to see how many full turns the main needle has made, then add the fractional reading from the large dial. If you are using a digital dial gauge, this process is simplified with a clear numerical display, though the mechanical principles remain the same.

Mounting Your Dial Gauge with a Magnetic Base

A dial indicator is only as accurate as its mounting. If the gauge moves even a hair during the process, your data is useless. This is why using a dial gauge magnetic stand is essential.

There are two primary ways to mount your dial gauge:

Stem Mounting: Clamping the stem directly with a screw or a split-body fastening. The mounting hole tolerance is typically ø8G7 (+0.005 to 0.02). Lug Mounting: Using the "lug" on the back of the gauge for specialized holders.
Stem Mounting Lug Mounting

When using a dial gauge with magnetic base, ensure the spindle is in line with the intended measurement direction to avoid "cosine-effect" errors.

How to Use Dial Gauge Tools for Maximum Accuracy

To get the most out of your mitutoyo dial gauge, follow these professional tips:

  • Avoid the Cosine Effect: If the measuring direction is misaligned with the intended direction of measurement, the reading will be inaccurate. Compensate for the angle if straight-on measurement is not possible.
  • Avoid the Cosine Effect
  • Cleanliness Matters: Before using the gauge, wipe the contact point and the workpiece. Even a tiny piece of dust can affect a 0.001 mm reading.
  • Spindle Care: Never lubricate the spindle with oil, as this can attract dust and cause malfunction. If movement feels sticky, clean the spindle with a dry or alcohol-soaked cloth.
  • Repeatability Check: Push the contact point quickly and slowly five times against a steady surface to ensure the needle returns to the exact same position each time.
  • Repeatability Check

Get Genuine Mitutoyo Precision at MISUMI

When accuracy is the foundation of your work, you cannot afford to use subpar tools. Mitutoyo is committed to delivering the latest technology in dimensional metrology, supported by world-class service. Whether you require a classic mechanical indicator or an advanced digital dial gauge, choosing a supplier you can trust is essential.

MISUMI offers an extensive range of genuine Mitutoyo dial gauge products and accessories, including dial gauge magnetic stands and replaceable contact points.

Ready to upgrade your measurement accuracy? Shop Mitutoyo Indicators and Accessories at MISUMI today.

Published By

Rupali Sharma

Share on:

whatsapp-qr whatsapp-icon