(!)NOTE : Windows 7 users won’t be able to use some latest features of eCatalog/WOS since Microsoft is ending support for Windows 7 on 14 Jan, 2020. Please upgrade your system for uninterrupted services.

  • Scheduled Maintenance Notice: This site will be unavailable due to scheduled maintenance from 13:30 5/4/2026 to 5:30 (IST) 6/4/2026. We apologize for the inconvenience.
Linear Shafts in Motion Systems

Common Linear Guide Problems and How to Fix Them

Categories:

Actuators

Publish Date: 6 Oct 2025

Linear guides are essential parts in many machines, robots, and automation systems. They help parts move smoothly and accurately in a straight line. But like all machine parts, linear guides can face problems that affect their performance.

1. Noise and Shaking

If your linear guide makes noise or shakes while moving, it might be because the rails are not lined up right, or dust and dirt are stuck inside.

Fix: Clean the rails gently with a soft cloth. Make sure the rails are straight and tightly fixed. Add the right lubricant to reduce noise.

2. Uneven Wear

Some parts of the guide may wear out faster if the load is not spread evenly or if you don’t lubricate regularly.

Fix: Check that the load is balanced on the guide. Apply grease or oil as recommended by the maker. Replace worn parts early.

3. Rails Not Aligned

If the rails or blocks are not aligned properly, the guide can wear quickly or move roughly.

Fix: Use a tool to check the alignment and adjust the rails. Tighten loose screws and allow small gaps for heat. Re-align guides regularly.

4. Lubrication Problems

Using wrong grease or putting too much or too little lubricant can cause damage.

Fix: Use the lubricant recommended for your guide type. Lubricate regularly but don’t overdo it. Automatic lubricators can help keep the right amount.

5. Dirt and Rust

If dirt or moisture gets into your guides, they can get damaged or rust.

Fix: Clean your guides often. Use covers or seals to protect from dust and water. Apply rust protection if necessary.

6. Early Breakdowns

Overloading or not taking care of your guides can cause parts to fail sooner.

Fix: Always use the guide within its load limits. Perform regular checks and replace old or damaged parts on time.

7. Rough or Uneven Movement

If the guide moves jumpy or unevenly, screws might be loose or parts may be blocked.

Fix: Tighten screws carefully. Check for and clear any dirt or obstacles. Make sure the load and preload settings are correct.

Simple Tips to Keep Linear Guides Working Well

  • Check and clean your guides regularly, especially in dusty places.
  • Use the right lubricant at the right time.
  • Keep rails straight; realign if needed.
  • Protect guides from dust, water, and chemicals.
  • Don’t overload; follow the weight limits.
  • Replace any parts that wear out quickly.

By following these easy steps, your linear guides will last longer and work smoothly, saving time and money.

Published By

Vishal Dhara

Share on:

whatsapp-qr whatsapp-icon