Types of Industrial Brushes Used in Food, Textile, and Electronics Conveyors
Publish Date: November 3, 2025
Industrial brushes play a vital role in maintaining conveyor systems across multiple industries, especially in food, textile, and electronics manufacturing. These brushes are designed to perform cleaning, polishing, static removal, and product handling tasks to ensure quality, safety, and operational efficiency. The type of brush used depends on the application environment, product type, and desired cleaning or finishing action.
This article highlights the main types of industrial brushes commonly used in conveyor systems and explains their roles in food, textile, and electronics industries.
1. Strip Brushes
Strip brushes consist of bristles mounted on a metal or plastic channel. They are used for sealing, guiding, and cleaning purposes in conveyors. The flexible bristles efficiently remove dust, crumbs, and fine debris without damaging delicate surfaces.
- Food Industry: Used for removing food particles from belts and maintaining hygiene between production cycles.
- Textile Industry: Prevent fiber accumulation and maintain fabric cleanliness.
- Electronics Industry: Reduce static buildup while gently cleaning circuit boards or components.
2. Cylindrical (Rotary) Brushes
Cylindrical brushes are mounted on rotating shafts and are used for continuous cleaning and surface treatment. Their rotation allows efficient removal of residues or contaminants while the conveyor is in motion.
- Food Processing: Clean conveyor belts or fruits and vegetables during packaging and inspection.
- Textiles: Remove lint and fibers from rollers or fabric surfaces.
- Electronics: Gently polish and clean printed circuit boards (PCBs) without static interference.
3. Spiral Brushes
Spiral brushes have bristles wound helically around a core and are used where continuous sweeping or cleaning motion is required. They are efficient for handling conveyor systems with curved or uneven surfaces.
- Food Conveyors: Used for removing moisture or debris from products before labeling or packing.
- Textile Conveyors: Ensure consistent fabric tension by clearing accumulated dust and fibers.
- Electronics Conveyors: Maintain static-free and dust-free environments for high-precision assembly lines.
4. Disk (Circular) Brushes
Disk brushes are circular in shape and used for targeted cleaning or polishing operations. They are commonly integrated into conveyor lines where space or cleaning precision is critical.
- Food Industry: Remove fine powder or residues from stainless steel or plastic belts.
- Textile Industry: Maintain roller cleanliness and improve yarn processing efficiency.
- Electronics Industry: Provide localized dust removal in component transfer systems.
5. Antistatic Brushes
Antistatic brushes are designed with conductive fibers that neutralize electrostatic charges during product movement. This is especially crucial in sensitive environments like electronics manufacturing.
- Electronics: Prevent static discharge that could damage circuit boards or sensors.
- Food: Minimize dust adhesion on plastic packaging films.
- Textiles: Prevent fiber sticking and improve material handling safety.
Brush Selection Guide for Conveyor Applications
| Brush Type | Primary Use | Typical Industries |
|---|---|---|
| Strip Brush | Dust and particle removal, sealing | Food, Textile, Electronics |
| Cylindrical Brush | Continuous belt cleaning | Food, Textile |
| Spiral Brush | Moisture or debris removal | Food, Textile |
| Disk Brush | Targeted cleaning, polishing | Food, Electronics |
| Antistatic Brush | Static removal, surface protection | Electronics, Textile |
Conclusion
The selection of the right industrial brush for conveyor systems depends on factors like product type, cleanliness standards, and operational conditions. From strip and spiral brushes in food conveyors to antistatic brushes in electronics assembly lines, each type serves a specific purpose that enhances system performance and product quality. Regular maintenance and proper brush material selection help extend conveyor life, ensure hygiene, and maintain consistent productivity across industries.