BLOCK DIES -GUIDE-

Block dies list

Block die type Material Type Without scrap retention With scrap retention
Round Shaped Round Shaped
Block, straight
Equivalent
to SKD11
Regular type BLD BLD□ SR-BLD SR-BLD□
Powdered
highspeed
steel
Regular type PBLD PBLD□ SR-PBLD SR-PBLD□
Block, single flange
Equivalent
to SKD11
Regular type BLDF BLD□F SR-BLDF SR-BLD□F
Powdered
highspeed
steel
Regular type PBLDF PBLD□F SR-PBLDF SR-PBLD□F
Block, straight, small type
Equivalent
to SKD11
Regular type SBLD SBLD□    
Powdered
highspeed
steel
Regular type SPBLD SPBLD□    
Block, single flange, small type
Equivalent
to SKD11
Regular type SBLDF SBLD□F    
Powdered
highspeed
steel
Regular type SPBLDF SPBLD□F    
Block, configurable size
Equivalent
to SKD11
Regular type FBLD FBLD□ SR-FBLD SR-FBLD□
Powdered
highspeed
steel
Regular type FPBLD FPBLD□ SR-FPBLD SR-FPBLD□
Block, fixingbolt
Equivalent
to SKD11
Regular type BBD BBD□ SR-BBD SR-BBD□

Indication of block die relief angle


indicates a taper in which the diameter increases by 1mm over 50mm of length.

Taper 1/50
Angle(A°) 1.146°

Dimension L of block die and spread of dimensions P and W(In case of )

Scrap retention block dies(For details, Click here)

Scrap retention block dies include two or more slanted grooves machined on the inner surface of the die.
The scrap initially punched out during the punching process forms small projections along the slanted grooves in the die. When the punching process pushes this scrap farther down to the bottom, the projections become compressed by the sides of the die("ironing" effect), preventing scrap lifting from occurring.

●Applicable range
   1. Hole diameter:φ1.0~φ16
   2. Workpiece material: Can be used for materials with tensile strengths up to
       1,177N/mm2 (120kgf/mm2)
   3. Thickness of workpiece materials: Minimum thickness 0.15 mm
   4. The scrap retention effect cannot be obtained if the clearance(C) exceeds 20%
       of the workpiece thickness(MT). Make sure that the clearance is 20% or less of MT.
Clearance(C)<Workpiece thickness(MT)×20%

Because scrap retention block dies prevent scrap lifting by forming small projections on punching scrap, they are not suitable in cases such as punching of precision holes, or when the punched-out item becomes the product.

How to order block dies
The position of the shaped hole can be determined as needed within the allowable range.

TOP

INDIA Stock List